Regarding hardware resizer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding hardware resizer

1,385 Views
shilpac
Contributor II

Hi,

We need to perform resize operation using hardware unit while encoding a video stream. But 'i.MX 6Dual/6Quad SABRE-AI Linux Release Notes, Rev. L3.0.35_1.1.0, 01/2013'  says

'IPU library is removed from i.MX 6. Should not use IPU library interfaces in i.MX 6 SW.'

Is there a way to perform re-sizing using hardware unit in 3.0.35 other than migrating to different kernel version ?

Set up details

Hardware: IMX6Q Sabrelite Eval Board

Release: Yocto 1.4

Build: Linux 3.0.35_1.1.0

Media Framework: GStreamer

Regards,

Shilpa Chandrappa

Labels (4)
0 Kudos
Reply
1 Reply

1,264 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shilpa,

please look at examples below

ipu-examples release notes - v0.1

Also suggest post this to meta-fsl-arm mailing list, so that someone very familiar with

hardware IPU resizing could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply