Regarding 24MHz Crystal of MCIMX6G3CVM05AA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding 24MHz Crystal of MCIMX6G3CVM05AA

842 Views
arvapallykumara
Contributor I

hello ,

we have gone through latest Freescale Design files(SPF-28617_C5) where we observed that resistor divider circuit at 24MHz crystal (pin T17 , XTALO ) the resistor values are 0 ohm and 499 ohm and we are also referring Freescale Design files(SPF-29105_C) where they are using resistor divider circuit as 1K and 2K ohm , and in Errata sheet (ERR009455 ) suggested to use 1K and 499 ohm.

we are in bit confusion which to use ,kindly suggest us which is right one

Please find the attachmed images for your reference .

regards,

Kumaraswamy

Labels (4)
0 Kudos
Reply
1 Reply

747 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello,

We suggest that you use the recommendation from the errata  (ERR009455 ) suggested to use 1K and 499 ohm.

As you can see in our latest reference design we use 2k and 1K to adjust the impedance regarding the Crystal but we recommend to use the 1K and 499 to start.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply