Reg Xenomai patch for IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reg Xenomai patch for IMX6

4,014 Views
shalinikp
Contributor II

I need to Add Xenomai Patch for  Yocto Kernel for IMX6 board. Please revert if anyone has done it. I need the procedure and how to chose the patch and from where do we get ?

Labels (4)
Tags (3)
0 Kudos
Reply
2 Replies

2,952 Views
jamesbone
NXP TechSupport
NXP TechSupport

The Support for this patch it is delivered from the people from Xenomai see ksrc/arch/arm/patches/README in Xenomai sources for instructions on how to use it.

Or visit their web page :

http://xenomai.org/getting-help/


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,952 Views
saurabh206
Senior Contributor III

Hi,

Shalini

First you need to study Yocto document for Kernel patch.

You need to create source\meta-*\recipe-kernel\

Thanks

Saurabh