Hello,
We are using IMx6 Dual Core CPU and 5.2inch FHD LCD in our Design. We have some clarfication regarding between LCD and IMX6 interface below please clarify us
Query 1:
IMx6 Dual CPU support MIPI 2 Lane Interface and our LCD support MIPI 4 Lane Interface, How i will Interface both (2Lane with 4 Lane)?
Query 2:
Whether any one know LVDS or HDMI to MIPI 4 Lane Converter Chip?
Host Interface: LVDS or HDMI
LCD Interface: MIPI 4 Lane
Best Regards
Sathiyan. D
Hello Sathiyan,
>>Query 1:
The max speed of MIPI DSI port on iMX6 is 2Gbps, and support XVGA/SVGA/WVGA/VGA/CIF/QCIF,QVGA/QQVGA resolution. For your LCD, you should check if it can work at 2-lane mode, I think it can.
>>Query 2:
LVDS to MIPI :DS90C387/DS90C388
HDMI to MIPI: TC358779XBG
Just provide 2 examples, you can evaluate them, or look for other chips!
Have a nice day!
Best regards,
Weidong
www.confuindustries.com
Specializing in HDMI to MIPI DSI EDP LVDS TTL RGB Interface Adapters RK3288 Dual Multi Displays. Applied for LCD OLED Display (2K 4K): VR HMD, Raspberry Pi,3D Printer, PC,TV, Car Displays, POS,PLC, Advertising Machine.
Confu HDMI TO MIPI DSI Tested Models (2K 4K, Singal / Dual Screens, Touch Function)
Brand Model Display Size Resolution(S) Resolution(Dual)
SHARP LS029B3SX02 LCD 2.89 1440*1440 2880*1440 70Hz
SHARP LS055T1SX01 LCD 5 1080*1920 NA 50-60Hz
SHARP LS055R1SX03 LCD 5.5 1440*2560 NA 50-60Hz
SHARP LS055R1SX04 LCD 5.5 1440*2560 NA 50-60Hz
SHARP LS060R1SX01 LCD 6 1440*2560 NA 50-60Hz
SHARP LS079L1SX02F LCD 7.9 1536*2048 NA 50-60Hz
JDI ACX450AKN-7 LCD 5 1080*1920 NA 50-60Hz
JDI ACX465AKM-7 LCD 5.9 1080*1920 NA 50-60Hz
JDI LPM055A138A LCD 5.5 1440*2560 NA 50-60Hz
JDI LPM055A184A LCD 5.5 1440*2560 NA 50-60Hz
JDI LT070ME05000 LCD 7 1200*1920 NA 50-60Hz
JDI TFTMD089030 LCD 8.9 2560*1600 NA 50-60Hz
AUO H546DLB01.2 OLED 5.5 1080*1920 NA 50-60Hz
AUO H381DLN01.2 OLED 3.81 1080*1200 2160*1200 90Hz
Everdisplay E295FMM1 OLED 2.95 1080*1200 2160*1200 90Hz
BOE NA LCD 3.5 1440*1600 2880*1600 60Hz
Samsung AMS567DJ01 OLED 5.67 1440*2560 NA 60Hz Note4
Sony Z5 4K AMS567DJ01 IPS 5.5 3840*2160 NA 30H