Reg: Audio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reg: Audio

1,901件の閲覧回数
vishvapathi
Contributor V

Hi All,

   I am using IMX 6Q, hardware-Mars board. I am working to interface audio to MArs board. All i need is to play audio in speakers, mic not necessary. I guess DAC is enough for my requirement. Can anyone suggest me  which hardware would suit my requirement.

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

1,688件の閲覧回数
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi,

To send audio to your speakers you will need a codec and, if the codec IC or speakers doesn't have one already, an amplifier. If you want to use headphones only, the amplifier is not needed.

I'm not familiar with the Mars board, but in our boards:

- ARD uses CS42888 for the ESAI interface.

- SDP uses WM8962 for the SSI interface.

This document may be useful: http://www.freescale.com/files/training_pdf/VFTF09_AA132.pdf.

Best regards.

Jorge.

0 件の賞賛
返信

1,688件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

You can take a look on Freescale boards, and see what hardware they use and mainly, how they connect things up.

I´m sorry, but I´m not a hardware girl, I cannot suggest you things.

Are you sure your board does not have a audio chip?

0 件の賞賛
返信

1,688件の閲覧回数
vishvapathi
Contributor V
0 件の賞賛
返信