Rebuild busybox failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Rebuild busybox failed

2,390 Views
yafeizhang
Contributor I

I want to enable some services like telnetd inetd crond.. I follow the blow steps, it do nothing.

1. $ bitbake -c menuconfig busybox

2. Unselect udhcpc and udhcpd.

    Save & exit

3. $bitbake -c diffconfig busybox

4. Create busybox_%.bbapend under directory:

    sources/poky/meta/recipes-core/busybox/

    Add below two lines in the file created above:

    FILESEXTRAPATHS_prepend := "${THISDIR}/${PN}:"
    SRC_URI += "file://fragment.cfg

5. Copy the file (fragment.cfg) created in step 3 to sources/poky/meta/recipes-core/busybox/

    Copy below to line to the file fragment.cfg

    CONFIG_UDHCPD=n
    CONFIG_UDHCPC=n

6. $bitbake <image>

 

And the build_8m_mini/tmp/work/aarch64-poky-linux/busybox/1.27.2-r0/busybox-1.27.2/.config  not modified  

it seems that every time I  $bitbake <image> , it unzip from downloads/busybox-1.27.2.tar.bz2.。

it appears .config.old  .config.orig , when and why?   it dose not contained by busybox-1.27.2.tar.bz2.

the two files cover the .config which generated by $ bitbake -c menuconfig busybox  when I $bitbake <image>. 

what should I do ,how to enable telnetd\inetd\crond 

busybox.png

0 Kudos
Reply
2 Replies

2,343 Views
yafeizhang
Contributor I

Blow is my  busybox_%.bbappend and fragment.cfg,I saw writing in two formats of busybox_%.bbappend 

Which one is correct?

append.png

append1.png

busybox.png

0 Kudos
Reply

2,343 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello yafei,

    When you change some source code or add some thing in a package of yocto,  and re-compile it, you should use "-f " parameter for bitbake command to force compilation.

    Such as:

$ bitbake -c -f menuconfig busybox

Try it, please!

Have a nice day!

B.R,

Weidong

0 Kudos
Reply