Reading Processor Variant and Fusemap from the console

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reading Processor Variant and Fusemap from the console

1,722 Views
yates
Contributor I

We are using the DART 6UL board from Varascite and their Yocto-generated 4.1.15 distribution. I have the following questions:

  1. Is there a way to read the processor variant (G0, G1, etc.), e.g., from the /proc file system (from the console)?
  2. How do you read the fuse map from the console? We want to read fuse map location 0x430, bits 21:20, "TAMPER_PIN_DISABLE[1:0]" (from the imx6 applications processor reference manual).

Namely I want to find out if the tamper inputs have been fused so that they cannot be used as GPIO outputs.

Thanks in advance for any pointers.

Labels (3)
Tags (2)
0 Kudos
Reply
1 Reply

1,599 Views
igorpadykov
NXP Employee
NXP Employee

Hi Randy

seems one can read the fuse map with: cat /sys/fsl_otp/

i.mx6ull GP3 & GP4 burning issue 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply