Re: iMX6 and eMMC 4.5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: iMX6 and eMMC 4.5

1,347 Views
mohamedkalilull
Contributor IV

Hello,

     MMC 4.4.1 is using in Customized imx6 board as boot device, after booting android (R13_04_ga), media files are detecting from MMC, SD, and USB taking long time also all applications taking long time for loading.

for eMMC is selected as default storage, changes are done in "vold.fstab" file,

if i select SD card as boot device, media files are detecting very fast, what are the changes i have to done for MMC?

Regards,

Kalil

Labels (2)
0 Kudos
Reply
0 Replies