Re: crash in libEGL with 3.10.17 BSP and wayland

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: crash in libEGL with 3.10.17 BSP and wayland

ソリューションへジャンプ
3,113件の閲覧回数
andyyang
Contributor II

Hi

I want to run 3D application which is developed by EGL/OpenGLES through weston-launch, it failed because the graphics driver is not right.

I check the error log and find that software call api[eglGetDisplay] and stop the application.

So i suspect that the whether libEGL-wl.so would have some question or not??

I have some questions for help.

1.Is DRM  must for weston(compositor),how to setup DRM?

2.Does GPU kernel drvier consist of kernel/driver/gpu/Vivante(Vivante.ko??) and of kernel/driver/gpu/drm/Vivante(DRM_Vivante.ko)?

3.Does user side drvier consist of EGL/OpenGLES?

4.graphics architecture is Application⇒EGL/OpenGLES/⇒libDRM⇒DRM_Vivante.ko⇒Vivante.ko⇒VIV-GPU?

[error info]

root:~> weston-simple-egl

[     1] HAL user version 4.6.9 build 6622 Aug 16 2013 11:28:30

[     2] HAL kernel version 4.6.9 build 1210

Segmentation fault (core dumped)

[CPU/GPU]

MCIMX6Qx/GPU-VIV

[EGL/GLES]

libEGL-wl.so

libGAL-wl.so

libGLESv2.so

[ref article]

Building Wayland-Weston for i.MX6

https://community.freescale.com/docs/DOC-95380

0 件の賞賛
返信
1 解決策
2,232件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,233件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
2,233件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Andy,

Do you already add the patches for the GPU,

i.MX 6 D/Q/DL/S/SL Linux 3.10.17_1.0.1 Patch Release?

0 件の賞賛
返信
2,233件の閲覧回数
andyyang
Contributor II

Hi Jamesbone

Thank you very much for your reply.

I will try to add this patch.

Meanwhile,let me confirm something.

I want to run wayland/weston on MCIMX6Qx/GPU-VIV target.

So i have to setup user space driver and kernek driver for GPU-VIV.

How can i get the freescale official release of user space driver and kernek driver for GPU-VIV?

Best regards.

0 件の賞賛
返信
2,233件の閲覧回数
andre_silva
NXP Employee
NXP Employee

Hi Andy,

the error you faced is due different GPU and kernel version, they have to match. If you get the old driver and try on a new kernel it will fail, the vice-versa also.

which BSP you are going to use ? LTIB or YOCTO ? in both cases you need to include the gpu-viv-bin package (in package list)  and also the wayland.

it will only be possible to use different version if you rebuild the gpu source code, what I think this is not the case.

regards,

Andre

0 件の賞賛
返信
2,233件の閲覧回数
YixingKong
Senior Contributor IV

Andy

The previous DI had been closed for some time. To make thing simple, I branch your post into this one, and will try to find an engineer to help you.

Thanks,

Yixing