Ram Size Increase - Android imx8mm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ram Size Increase - Android imx8mm

1,415件の閲覧回数
seanlink
Contributor I

We are working on a product that is closely modeled after the imx8mm_evk. Due to increased memory demand, we decided to increase the amount of RAM from 2GB to 3GB. Android is able to boot with only one change within uboot.

include/configs/imx8mm_evk.h

-  #define PHYS_SDRAM_SIZE 0x80000000 /* 2GB DDR */
+ #define PHYS_SDRAM_SIZE 0xC0000000 /* 3GB DDR */

 

I was wondering why I didn't need to make any changes to the device tree itself? Shouldn't this have crashed or failed to compile if the deivce tree was not updated? Am I going to get into any trouble without updating the device tree?

 

Section to update in question

arch/arm/dts/imx8mm-evk.dts

memory@40000000 {
    device_type = "memory";
    reg = <0x0 0x40000000 0 0x80000000>;
};

 

0 件の賞賛
返信
1 返信

1,397件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Am I going to get into any trouble without updating the device tree?

-->No, The DRAM has been initialized in SPL. It doesn't use dts in this stage.

0 件の賞賛
返信