RTSP Server Setup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTSP Server Setup

3,534 Views
parveenkumaryad
Contributor III

Hi all,

I am Working on a customize project with imx6qd processor. I am using YOCTO 1.6 daisy framework. i am using linux kernel 3.10.17 .

I want to stream video+Audio from our IMX board to PC through wifi.

For that i want to set-up an RTSP-Server in our project. I am using gstreamer in the project for playing and streaming video.

I am able to stream using TCP and UDP but both of them have their own disadvantages.

Can any provide the steps to setup the server and also the gstreamer commands to stream video and audio.

Labels (4)
0 Kudos
Reply
3 Replies

3,196 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Have you checked this discussion? It may have some useful information for you.

Regards,

Alejandro

0 Kudos
Reply

3,196 Views
parveenkumaryad
Contributor III

hi Alejandro

You have forget to share the link of the discussion.

Regards

Parveen

0 Kudos
Reply

3,196 Views
alejandrolozan1
NXP Employee
NXP Employee

Sorry,

RTSP gstreamer and vpudec

I hope that helps,

Alejandro

0 Kudos
Reply