RT1064 how to use PWMX module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1064 how to use PWMX module

1,354 Views
Alexander-cloud
Contributor I

Because of some requirements of the project, I use the PWMX module of flexPWM to control GPIO_AD_B0_02 to output PWM. The reference manual says that no mapping is required, and PWM can be output directly, but I found that I have no way to start. The examples in the manual are not as detailed as other modules, and my strength is limited. , please help me find out what to do. thanks

0 Kudos
Reply
1 Reply

1,312 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi Alexander,

Thank you so much for using our community.

I suggest you, refer to the evkmimxrt1064_pwm SDK example and with the help of Config Tools you can configure that pin you want, you would only have to make slight configuration modifications.

I hope this will help you. Please let me know if you have more questions about it.

0 Kudos
Reply