RT1064 how to use PWMX module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1064 how to use PWMX module

1,347 次查看
Alexander-cloud
Contributor I

Because of some requirements of the project, I use the PWMX module of flexPWM to control GPIO_AD_B0_02 to output PWM. The reference manual says that no mapping is required, and PWM can be output directly, but I found that I have no way to start. The examples in the manual are not as detailed as other modules, and my strength is limited. , please help me find out what to do. thanks

0 项奖励
回复
1 回复

1,305 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi Alexander,

Thank you so much for using our community.

I suggest you, refer to the evkmimxrt1064_pwm SDK example and with the help of Config Tools you can configure that pin you want, you would only have to make slight configuration modifications.

I hope this will help you. Please let me know if you have more questions about it.

0 项奖励
回复