RT1050 supported memories

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1050 supported memories

2,988件の閲覧回数
mbuckley
Contributor II

Is there a list of SDRAM and flash devices that are supported by the RT1050 beyond those that are on the development board?

タグ(3)
0 件の賞賛
返信
5 返答(返信)

2,756件の閲覧回数
gordonmacnee
Contributor I

Firstly I must confess a bias in that I work for Adesto Technologies. That done, Adesto have a 32Mbit (4MByte) Flash memory designed to work with the i.MX1050. The EcoXiP ATXP032 has an OCTAL interface and can offer a peak transfer rate of 266MBytes/s. We are also planning larger memory devices later this year. These parts are fitted to the Embedded Artists i.MX RT1050 board and there are some videos discussing performance and power consumption from EA on Youtube.    

0 件の賞賛
返信

2,756件の閲覧回数
mbuckley
Contributor II

Hi Igor,

Thank you for the reply.  I believe you are saying that there is no list of specific devices that are supported (i.e. part numbers) but there is a list of types of devices (i.e. SDRAM, NAND flash, SRAM, etc.) in the manual and datasheet. Is that correct?

Thanks,

Matt

0 件の賞賛
返信

2,756件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Matthew

yes correct.

Best regards
igor

0 件の賞賛
返信

2,756件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Matthew

I am afraid such list is not available and one can follow

formal description of supported devices in datasheet and reference manual.

https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf 

https://www.nxp.com/docs/en/data-sheet/IMXRT1050CEC.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,260件の閲覧回数
oswald
Contributor I

Hi,

RT1050 reference manual shows SDRAM interface supports 512Mbit per each CS. and there are 4 CSs.

Is this mean RT1050 support 1 x 1Gbit SDRAM or 2 x 512Mbit SDRAM ?

Does RT1050 support 1Gbit external SDRAM ?

Thanks,

Oswald

0 件の賞賛
返信