RT1024 WATCHDOG TIMER 1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1024 WATCHDOG TIMER 1

1,186件の閲覧回数
Gaetan
Contributor II

Hello,

We have installed watchdog timer 1 in our application.
It works correctly, but debugging has some issues.
The breakpoints work fine, but the single-step mode is giving an error.

Gaetan_0-1745855857233.png

our watchdog configuration :

Gaetan_1-1745855894280.png

SDK 2.15
MCUXpresso 11.9.1

0 件の賞賛
返信
3 返答(返信)

1,156件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Gaetan,

Do you see issues with single step only when watchdog is enabled? Or also when it is disabled? What debugger are you using (MCU-Link, J-Link, etc.)? Are you certain this debugger is updated to the latest firmware version? Please try updating your debugger to the latest version.

BTW, speaking of latest firmware versions, note that SDK 2.15 is over a year old now and might have bugs or issues. I highly recommend you update to the latest SDK version (25.03.00). In order to use this SDK, you will also require the latest IDE version (v24.12.148).

BR,
Edwin.

0 件の賞賛
返信

1,070件の閲覧回数
Gaetan
Contributor II

Unfortunately, our project is too advanced for us to afford to change IDEs or SDKs.
We use the MCU-LINK debugger.
We only observe the problem with the watchdog active and only with watchdogs 1 and 2.
We don't have the problem if we use the RT watchdog (watchdog 3).

0 件の賞賛
返信

1,040件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Gaetan,

I understand that you are not able to upgrade SDK on this specific project. In this case, I would recommend you stick to the WDT that does not show this error (WDT3 in this case).

BR,
Edwin.

0 件の賞賛
返信