RT1021 hangs in plugin when authentication fails when HAB config is open

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1021 hangs in plugin when authentication fails when HAB config is open

1,025 Views
rshipman
Senior Contributor I

Hi,

I have noticed that the RT1021 hangs when the plugin tries to write to the plugin api arguments (start, bytes, ivt_offset) if authentication fails, when the HAB closed fuse (SEC_CONFIG ) has not been blown - i.e. HAB configuration is 'open'.

I have blown the SRK_HASH fuses and can create a signed version of the plugin and app. When both are signed the plugin runs ok, copies the app to sdram, sets the plugin api arguments and returns back to the ROM. The ROM then runs the app. This all works fine when signed. When unsigned the boot plugin still runs, but as soon as it tries to set the api arguments, before returning, the RT1021 seems to hang. It has not reached the return. It is the setting of the arguments that is the problem. The copy to sdram works fine.

I can understand this behaviour if the RT1021 is HAB closed (SEC_CONFIG[1] set to 1). According to the documentation, the HAB should not prevent execution if SEC_CONFIG[1] is 0

So why is this happening when the HAB configuration is open?

See:
Document: i.MX RT1020 Processor Reference Manual, Rev. 2, 01/2021
Section 9.2 Overview:
"The out-of-fab setting for the SEC_CONFIG is the open configuration, in which the ROM/HAB performs the image authentication, but all authentication errors are ignored and the image is still allowed to execute."

Section: 9.8 Plugin image
typedef BOOLEAN (*plugin_download_f)(void **start, size_t *bytes, UINT32 *ivt_offset);
ARGUMENTS PASSED:
start - the image load address on exit.
bytes - the image size on exit.
ivt_offset - the offset (in bytes) of the IVT from the image start address on exit.
RETURN VALUE:
1 - success
0 - failure

Plugin snippet:
*start = APP_BINARY_DESTINATION_ADDRESS;
*bytes = APP_BINARY_SIZE;
*ivt_offset = 0x1000;
return 1;

Kind regards,

Ronnie

Labels (1)
0 Kudos
Reply
1 Reply

1,014 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) So why is this happening when the HAB configuration is open?
-- Before answering your question, I think I need more information, as I was wondering if you can list the testing steps and related results in detail.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply