RPMsg Framework queries

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RPMsg Framework queries

1,806 Views
sharmila_devada
Contributor III

Hi,
 I am using RPMsg Framework for Communication between Cortex-A35 core to Cortex-M4 core.
Below are my queries :
1. I have created multiple endpoints for a single channel. I have increased the buffer size (RPMSG_BUF_SIZE ) to 1024. This buffer is for Single endpoint (In single endpoint we can have 1024 bytes of data transfer) OR It is for the channel ?
2. From the documents I got to know that we even can create multiple channels. What is the advantages of having multiple channels ?
3. Can you please provide the information on Transmission rate, baud-rate and throughput details of RPMsg data transfer.
4. What is the known limitation of RPMsg framework ?
 Please provide the response for the above query
Thank you,
 Regards,
 Sharmila d

0 Kudos
Reply
1 Reply

1,577 Views
abhinav_warrier
Contributor I

Hi Sharmila I have answered most of your queries and have a working example for the Rpmsg stack 
Please check out this repository : GitHub - warrierabhinav/rpmsglite_nanopb_imx8: This is a unique communication stack which uses RPMSG... 

0 Kudos
Reply