RPMSG COMMUNICATION IN IMX7DSABRESD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RPMSG COMMUNICATION IN IMX7DSABRESD

3,516件の閲覧回数
nagaprasadvasam
Contributor III

Hi Everyone,

   I am booting Linux kernel version 4.9.88_2.0.0 for my imx Board, i need to enable inter-processor communication between m4 & A7 cores, i manually loaded modules related to RPmsg but a i am not getting any node for RPmsg inside /dev folder i.e /dev/ttyRPMSG how to enable it,can any one help me.

Thanks & Regards,

Prasad.

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,987件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi nagaprasad

one can try procedures described in sect.2.6 Remote Processor Messaging, sect.9.19

Remote Processor Messaging attached Linux Manual

rpmsg\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,987件の閲覧回数
nagaprasadvasam
Contributor III

Hi igor,

   Thanks for your reply, i have seen link you provided.but for that it is required that there should be a node in /dev i.e,

"/dev/ttyRPMSG". i am not able to get this when i loaded modules in imx7dsabresd.

Thanks & Regards,

Prasad.

0 件の賞賛
返信

2,987件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prasad

could you try with Demo Images from

i.MX Software|NXP 

for example Linux Binary Demo Files - i.MX 6UltraLite, i.MX 6ULL, i.MX 7Dual

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_MX6UL7D&appType=license&location=null&Pare... 

Best regards
igor

0 件の賞賛
返信