RNDIS class device USB connectivity issue on imx28evk board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RNDIS class device USB connectivity issue on imx28evk board.

3,159 Views
pradeeparora
Contributor I

Hi,

   I'm trying to connect a Lantronix xPico WiFi based board via USB to the imx28evk board. The peripheral board has been configured to present itself as an RNDIS class device.

   When I hook this up to my host machine running Ubuntu 14.04, the connection is successful. dmesg output is as follows:

> [16134.647582] usb 3-1.5.4: new full-speed USB device number 13 using xhci_hcd

> [16134.753271] usb 3-1.5.4: New USB device found, idVendor=0525, idProduct=a4a2

> [16134.753275] usb 3-1.5.4: New USB device strings: Mfr=1, Product=2, SerialNumber=3

> [16134.753277] usb 3-1.5.4: Product: Gadget RNDIS v2.4

> [16134.753279] usb 3-1.5.4: Manufacturer: ELMO GMAS

> [16134.753281] usb 3-1.5.4: SerialNumber: 123

  

When I connect the device to the imx28evk board (running kernel version 3.18.5-fslc built using the Yocto environment), dmesg yields the following:

[   60.035311] usb 1-1: new full-speed USB device number 2 using ci_hdrc

[   75.155258] usb 1-1: device descriptor read/64, error -110

[   75.461265] cdc_subset: probe of 1-1:1.0 failed with error -22


I suspect this to be a kernel configuration related issue. A couple of other pieces of information from the imx28evk target:

   1. CONFIG_USB_ETH_RNDIS has been enabled

   2. lsusb does recognize the device:

       Bus 001 Device 002: ID 0525:a4a2 Netchip Technology, Inc. Linux-USB Ethernet/RNDIS Gadget


Any assistance in resolving this issue would be greatly appreciated.



Regards,


Pradeep.

Labels (3)
Tags (1)
0 Kudos
Reply
1 Reply

1,620 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Pradeep,

In this case, an option could be contacting to the manufacturer of the Wi-Fi card in order to ask them if they have a specific Linux driver.

Hope this information will be useful for you.

Best regards!

/Carlos

0 Kudos
Reply