RMII interface on i.MX6 DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RMII interface on i.MX6 DL

767 Views
Lt1233
Contributor II

Hi,

I am using RMII between IMX6DL MAC and BCM5221KPTG PHY. My clock generation is the following( using 50MHz CLOCK Buffer with  1 input and 2 outputs as shown below:

 

Osc_50MHz----->CLK_BUF ----#1----> PHY(REF_CLK)

                                                |

                                                | ----#2----> IMX6DL.GPIO_16 (RMII_REF_CLK)

 

What are the Layout rules that need to be followed as far as RMII length matching?

1. Does Connection 1 (CLK_BUF-->PHY_REF_CLK) need be length match to connection 2 above(CLK_BUF-->GPIO_16) ?

2.Does TXD1,TXD0 and TX_CTL need be length match as a group?

3. Does RXD1, RXD0 and RX_CTL need be length match as a group?

4. Does the TXD group above need to be length matched to the RXD group above?

 

Thanks,

LT

0 Kudos
Reply
0 Replies