RAUC Integreation with Yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RAUC Integreation with Yocto

3,708 Views
MichaelBMiner
Contributor IV

Has anyone successfully integrated RAUC? Here is where I am at. 

 

In my local.conf I have added:

DISTRO_FEATURES_append = " systemd"
VIRTUAL-RUNTIME_init_manager = "systemd"
DISTRO_FEATURES_BACKFILL_CONSIDERED = "sysvinit"
DISTRO_FEATURES += "rauc"
MACHINE_FEATURES:append = " pcbios efi"

I created a basic bundle from an example I found:

DESCRIPTION = "RAUC bundle generator"

inherit bundle

RAUC_BUNDLE_COMPATIBLE = "${MACHINE}"
RAUC_BUNDLE_VERSION = "${DISTRO_VERSION}"
RAUC_BUNDLE_DESCRIPTION = "Generic Demo Bundle"
RAUC_BUNDLE_SLOTS = "rootfs"
RAUC_SLOT_rootfs = "core-image-minimal"
RAUC_SLOT_rootfs[fstype] = "ext4"

RAUC_KEY_FILE = "${THISDIR}/files/development-1.key.pem"
RAUC_CERT_FILE = "${THISDIR}/files/development-1.cert.pem"

Created rauc_%.bbappend as instructed (system.conf is currently empty):

FILESEXTRAPATHS:prepend := "${THISDIR}/files:"
SRC_URI:append := " file://system.conf"

 Told my application about the new layer/recipe:

IMAGE_INSTALL_append = " rauc \
generic-bundle "

 With this my first issue is 

ERROR: Nothing RPROVIDES 'grub-efi' (but /mnt/WorkDrive/Documents/MAIN_Application/sources/poky/meta/recipes-core/packagegroups/packagegroup-core-boot.bb RDEPENDS on or otherwise requires it)
grub-efi was skipped: incompatible with host arm-poky-linux-gnueabi (not in COMPATIBLE_HOST)

This seems to be a version issue, but how do I solve it?

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

3,686 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

3,699 Views
MichaelBMiner
Contributor IV

Update 1:

If I do not install my bundle and install rauc I am given an error during rootfs. 

ERROR: mainapplication-dev-1.0-r0 do_rootfs: Unable to install packages. Command '/mnt/WorkDrive/Documents/main_Application/build-fb/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/mainapplication-dev/1.0-r0/recipe-sysroot-native/usr/bin/opkg --volatile-cache -f /mnt/WorkDrive/Documents/main_Application/build-fb/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/mainapplication-dev/1.0-r0/opkg.conf -t /mnt/WorkDrive/Documents/main_Application/build-fb/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/mainapplication-dev/1.0-r0/temp/ipktemp/ -o /mnt/WorkDrive/Documents/main_Application/build-fb/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/mainapplication-dev/1.0-r0/rootfs  --force_postinstall --prefer-arch-to-version   --add-ignore-recommends udev-hwdb install base-passwd boost bridge-utils can-utils crccalculator crda dbcppp debugconfigs dhcpcd dtc ethtool maincan mainconfigs iperf3 isose iw kernel-module-lwb5p-backports-laird kernel-modules laird-localize-firmware libgpiod libsocketcan logrotate lumissil lumissil-kernel-module lwb5plus-sdio-sa-firmware open-plc-utils openssl packagegroup-core-boot packagegroup-core-eclipse-debug packagegroup-core-ssh-openssh rauc run-postinsts shadow socat stress-ng stressapptest sudo systemd-analyze tcpdump udevrules wireless-regdb-static wireless-tools wpa-supplicant' returned 255:
Disfavor package: udev-hwdb
Installing base-passwd (3.5.29) on root
0 Kudos
Reply

3,329 Views
Phil_liu
Contributor I

@Zhiming_Liu  Have any update for this error ? because , our custoemr also need to add RAUC in the BSP. thanks. 

0 Kudos
Reply