RAM speed on MX53

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RAM speed on MX53

1,087 次查看
docobo
Contributor I

Hi,

The datasheet and RM both state that the max clock requency for DDR3 RAM is 400MHz (can be written as DDR3-800 due to the double data rate) but the hardware reference manual for the quick start board (IMX53QSBRM.pdf) says that the SDRAM should be rated for 1066MHz or faster (chapter 5.5 "DDR3 SDRAM Memory").

Can anyone explain this discrepency?

Thanks

标记 (1)
0 项奖励
回复
0 回复数