Questions about the IPU capabilities of imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions about the IPU capabilities of imx6q

Jump to solution
3,158 Views
LeviathanSteven
Contributor III

Hi,

Recently I was working on imx6q.

From IMX6DQRM_revC.pdf, we know that imx6q has two IPUs, and each IPU has two DIs. So it seems that it can support 4 independent outputs simultaneously. I gave my understanding in the figure below.

imx6q_TVWall.JPG                                                                                                                   If the definition of this figure is not high enough for reading, please get the original picture from the attachment.

My questions is, Can we connected four transmitters(LVDS or HDMI) to all the four DIs, and  then connected four display monitors.  Can they worked   independently and  simultaneously.If yes, what's the HW limitation? Such as can we set each of the display monitors to 1920x1080p@60???

Actually this application is a TV Wall, which need four channels input   simultaneously.

Or any other suggestions?

Thanks so much in advance!                                                                                        

Labels (3)
Tags (3)
0 Kudos
Reply
1 Solution
2,804 Views
Yuri
NXP Employee
NXP Employee

Please look at my comments below.

1.

> Is that means for each DI, the sum of the connected two monitor's timing's pixel clocks can not be larger than 240M ?

Basically - yes. Let me remind MP/sec relates to Pixels / sec, so it is the same as display frequency, when
single clock is needed per pixel.  

2.

> For example, we can connected four monitors with mode 1280x1024@60 to the SOC, because the pixel clock

> of 1280x1024@60 is 108M, and two of them are 216M, which is smaller than 240M. In this case, the four monitors

> can work well simultaneously, which is as shown on the figure in my last mail.

> Am I right???

Yes, but again, please do not forgot, that these rates refer only to screen refresh, gated by the capabilities of the

display port. A full use case typically includes additional activities.

View solution in original post

0 Kudos
Reply
5 Replies
2,804 Views
Yuri
NXP Employee
NXP Employee

Basically it is possible to connect up to four displays (two displays per IPU) to i.MX6Q.
But performance restriction is as following : combined rate for the two ports is up to 240 MP/sec.  

As for 1920x1080p@60 mode - it requires ~120 MP/sec/. Looks like enough, but note  these rates

refer only to screen refresh, gated by the capabilities of the display port. A full use case typically

includes additional activities.

0 Kudos
Reply
2,804 Views
LeviathanSteven
Contributor III

Hi Muhin,

Thanks for your kindly help!

'But performance restriction is as following : combined rate for the two ports is up to 240 MP/sec. ' .

Is that means for each DI, the sum of the connected two monitor's timing's pixel clocks can not be larger than 240M ?

For example, we can connected four monitors with mode 1280x1024@60 to the SOC, because the pixel clock of 1280x1024@60 is 108M, and two of them are 216M, which is smaller than 240M. In this case, the four monitors can work well simultaneously, which is as shown on the figure in my last mail.

Am I right???

Sorry for bothering you,  but I just want to double confirm. Thanks.

0 Kudos
Reply
2,805 Views
Yuri
NXP Employee
NXP Employee

Please look at my comments below.

1.

> Is that means for each DI, the sum of the connected two monitor's timing's pixel clocks can not be larger than 240M ?

Basically - yes. Let me remind MP/sec relates to Pixels / sec, so it is the same as display frequency, when
single clock is needed per pixel.  

2.

> For example, we can connected four monitors with mode 1280x1024@60 to the SOC, because the pixel clock

> of 1280x1024@60 is 108M, and two of them are 216M, which is smaller than 240M. In this case, the four monitors

> can work well simultaneously, which is as shown on the figure in my last mail.

> Am I right???

Yes, but again, please do not forgot, that these rates refer only to screen refresh, gated by the capabilities of the

display port. A full use case typically includes additional activities.

0 Kudos
Reply
2,804 Views
LeviathanSteven
Contributor III

Hi Muhin,

OK, I got it!

Thanks so much for your great help!

0 Kudos
Reply
2,804 Views
LeviathanSteven
Contributor III

Any one can help? Can we connect four monitors to the two IPUs???

0 Kudos
Reply