Questions about camera specifications for i.MX8M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about camera specifications for i.MX8M

2,551件の閲覧回数
jihyun_seong
Contributor I

Dear, all

I'd like to know below camera specifications for i.MX8M

1) What's the maximum camera supported resolution for snapshot (still shot)? 

For example) jpeg, 2592x1944

As far as I know, ov5640 (it's mounted on i.MX8M Evk) support 5MP resolution. Does i.MX8M also support the maximum resolution of the camera sensor?

2) What's maximum video recording resolution/frame rate?

As I know i.MX8M support 1080p/30fps and H.264 S/W encoder only.  Is it the same as the camera preview usecase?

Thanks you.

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,352件の閲覧回数
jihyun_seong
Contributor I

Dear Rita,

Thanks for answering all my questions!

0 件の賞賛
返信

2,352件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

It's my pleasure. If you have new questions you can create new threads and contact us.

Have a nice day

Rita

0 件の賞賛
返信

2,352件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

2) There is no maximum video recording resolution/frame rate in software. They are not  the same. The maximum video recording resolution/frame rate is depending on your using.

0 件の賞賛
返信

2,352件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

1)Yes,You are right. The maximum resolution is 2592x1944. Details you can see the document https://www.nxp.com/doc/AN12187 .

Have a great day,
Rita

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信