Questions about IMX8 two LVDS displays

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about IMX8 two LVDS displays

1,374件の閲覧回数
RobbieJiang
Contributor IV

We have a IMX8QM board with Linux 4.19.35.

And the system have two LVDS interface (LVDS-1, LVDS-2) connected to two 800x400 LCD panel separately.

Each LVDS display works well with 'modetest' cmd.

E.g, 

modetest -M imx-drm -s 149@65:1280x768-60 //LVDS1

OR 

modetest -M imx-drm -s 151@123:800x480-60 //LVDS2

However, it is impossible to show the test pattern image on two LVDS panels SIMULTANEOUSLY.

My questions are:

1. How to make two LVDS interfaces work at the same time?

2. No frame buffer device (/dev/fb*) for my display devices.

The rootfs is built from yocto (bitbake imx-image-multimedia),

and only one frame buffer device (/dev/fb0) appears. 

How to enable frame buffer devices for two LVDS interfaces?

 

Regards,

Robbie

 

 

0 件の賞賛
返信
1 返信

595件の閲覧回数
Wobaffet
Senior Contributor I

Is frame buffer supported by the imx8 series?

0 件の賞賛
返信