Question on DDR calibration script

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question on DDR calibration script

2,881 Views
t_kuha
Contributor I

I noticed there are two different tools for DDR calibration:

- DDR3 Register Programming Aid (i.MX6DQ SABRE SDP/B DDR3 Register Programming Aid)

- i.MX6DQSDL DDR3 Script Aid ( i.MX6DQSDL DDR3 Script Aid)

What is the difference between them?

Which one should be used if I want to determine DDR initialization values to be used in u-boot?

Regards,

Labels (2)
0 Kudos
Reply
3 Replies

2,345 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Here recommend you to use the - i.MX6DQSDL DDR3 Script Aid ( i.MX6DQSDL DDR3 Script Aid). It's newer and have more option than the other one. When you open the link you can see the details.

DDR3 Script.PNG

The - DDR3 Register Programming Aid (i.MX6DQ SABRE SDP/B DDR3 Register Programming Aid) is only for MX6Q_SabreSD_DDR3_register.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,345 Views
t_kuha
Contributor I

Rita,

Thank you for the answer!

Regards,

0 Kudos
Reply

2,345 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

It's my plesure.

Have a nice day

Rita

0 Kudos
Reply