Question, i.MX8M Hardware design(27M clock)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX8M Hardware design(27M clock)

2,049 Views
SLICE
Contributor IV

Dear team,

I would like to ask about i.MX8M board design.

Can one remove an oscillator routed to XTALI_27M when HDMI of i.MX8M is not used?

Thanks,

Miyamoto

0 Kudos
Reply
3 Replies

1,754 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Generally 27M crystal may be used by other function like audio.

Only differential 27M oscillator can be removed if no HDMI function. 

Regards,

Yuri.

0 Kudos
Reply

1,754 Views
SLICE
Contributor IV

Hi Yuri‌

Thanks for your support.

Do you mean that ‘differential 27M oscillator’ is clock inputs to HDMI_REFCLK_P/N?

And HDMI_REFCLK_P/N can be left open when HDMI is not used.

And 27M crystal cannot be removed even if user does not use HDMI.

Correct?

 

BR,

Miyamoto

0 Kudos
Reply

1,754 Views
Yuri
NXP Employee
NXP Employee

Correct!

~Yuri.

0 Kudos
Reply