Question, i.MX8M Hardware design(27M clock)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX8M Hardware design(27M clock)

2,060件の閲覧回数
SLICE
Contributor IV

Dear team,

I would like to ask about i.MX8M board design.

Can one remove an oscillator routed to XTALI_27M when HDMI of i.MX8M is not used?

Thanks,

Miyamoto

0 件の賞賛
返信
3 返答(返信)

1,765件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  Generally 27M crystal may be used by other function like audio.

Only differential 27M oscillator can be removed if no HDMI function. 

Regards,

Yuri.

0 件の賞賛
返信

1,765件の閲覧回数
SLICE
Contributor IV

Hi Yuri‌

Thanks for your support.

Do you mean that ‘differential 27M oscillator’ is clock inputs to HDMI_REFCLK_P/N?

And HDMI_REFCLK_P/N can be left open when HDMI is not used.

And 27M crystal cannot be removed even if user does not use HDMI.

Correct?

 

BR,

Miyamoto

0 件の賞賛
返信

1,765件の閲覧回数
Yuri
NXP Employee
NXP Employee

Correct!

~Yuri.

0 件の賞賛
返信