Question, i.MX6SoloX U-Boot with eMMC fastboot enabled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX6SoloX U-Boot with eMMC fastboot enabled

1,488件の閲覧回数
SLICE
Contributor IV

Dear team,

Let me ask about how to build U-Boot with enabling eMMC Fast boot mode.

My customer is facing to build u-boot.

They want to be sure that the u-boot has a feature for load kernel image with eMMC fastboot.

They found a definition of “CONFIG_FSL_FASTBOOT” in your u-boot source code including your following BSP code. (in mx6sxsabresd.c)

git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.52-1.1.0_ga

And they think that CONFIG_FSL_FASTBOOT should be defined for u-boot to have a feature to load kernel image with eMMC fastboot.

Is it true?

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 返信

1,181件の閲覧回数
art
NXP Employee
NXP Employee

Actually, this feature is still not confirmed as being reliably supported in the current versions of software, so, it is not recommended to use it at all.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信