Question, i.MX6Q DDR3 selection.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX6Q DDR3 selection.

1,067件の閲覧回数
SLICE
Contributor IV

Dear team,

I would like to ask about DDR controller of i.MX6Q.

My customer wants to use DDR3-800 instead of DDR3-1066 for their board because of its distribution amount.

If you have any concern on that, please let me know.

The customer concerns if there is any restrictions on margin for selecting DDR chip.

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 返信

978件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   It is needed to configure memory frequency for 400 MHz, when using DDR3-800.

https://community.nxp.com/docs/DOC-105963 

i.MX6/7 DDR Stress Test Tool V2.60 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信