Question, i.MX28 LRADC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question, i.MX28 LRADC

跳至解决方案
1,920 次查看
Aemj
Contributor IV

Hi Team,

I would like to ask about LRADC of i.MX28.

From the description in i.MX28 datasheet, the power source of LRADC seems to be VDDA. Right?

And the datasheet says that the maximum voltage of LDRADC is 1.85V.

(1)

Is it possible for LRADC to operate correctly for 1.85V input to LRADC, in the situation that VDDA is lower than 1.85V?

(2)

The reference voltage, the internal Bandgap reference, for the ADC is always 1.85V?

Thanks,

Miyamoto

标签 (1)
0 项奖励
回复
1 解答
1,657 次查看
art
NXP Employee
NXP Employee

Q. From the description in i.MX28 datasheet, the power source of LRADC seems to be VDDA. Right?

A. No, this is not right. The supply voltage for LRADC is fed directly from the Power Supply module, it is derived from either Battery or V4P2 voltage by a linear regulator.

Q. Is it possible for LRADC to operate correctly for 1.85V input to LRADC, in the situation that VDDA is lower than 1.85V?

A. As told before, VDDA does not affect the LRADC operation. So, the answer is: yes, it is possible for LRADC to operate correctly for 1.85V input to LRADC, in the situation that VDDA is lower than 1.85V.

Q. The reference voltage, the internal Bandgap reference, for the ADC is always 1.85V?

A. Yes.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,658 次查看
art
NXP Employee
NXP Employee

Q. From the description in i.MX28 datasheet, the power source of LRADC seems to be VDDA. Right?

A. No, this is not right. The supply voltage for LRADC is fed directly from the Power Supply module, it is derived from either Battery or V4P2 voltage by a linear regulator.

Q. Is it possible for LRADC to operate correctly for 1.85V input to LRADC, in the situation that VDDA is lower than 1.85V?

A. As told before, VDDA does not affect the LRADC operation. So, the answer is: yes, it is possible for LRADC to operate correctly for 1.85V input to LRADC, in the situation that VDDA is lower than 1.85V.

Q. The reference voltage, the internal Bandgap reference, for the ADC is always 1.85V?

A. Yes.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复