Dear team,
I would like to ask about i.MX1.
My customer is using SSI2_RX and SSI2_TXCLK of i.MX1 as input from external.
They need to know the specification of the input waveform, especially rise/fall time, for the signals but they could not found the specification in i.MX1 datasheet.
Actually, the signals that flow into those pins have 25ns of rise/fall time on their board.
Could you show me whether the 25nS of rise/fall time is acceptable?
Thanks,
Miyamoto
解決済! 解決策の投稿を見る。
Hi AVNET JAPAN FAE
rise/fall times are not specified, because they are not important.
Important are setup and hold times, these and other important parameters
are provided in datasheet.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi AVNET JAPAN FAE
rise/fall times are not specified, because they are not important.
Important are setup and hold times, these and other important parameters
are provided in datasheet.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor,
Thanks for your prompt reply.
Can i understand 25nS of rise/fall time is OK?
My customer wants your comment on the rise/fall time.
BR,
Miyamoto
Hi Miyamoto
yes this rise/fall time is OK.
~igor