Question, i.MX1 SSI signal timing specification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX1 SSI signal timing specification

Jump to solution
766 Views
Aemj
Contributor IV

Dear team,

I would like to ask about i.MX1.

My customer is using SSI2_RX and SSI2_TXCLK of i.MX1 as input from external.

They need to know the specification of the input waveform, especially rise/fall time, for the signals but they could not found the specification in i.MX1 datasheet.

Actually, the signals that flow into those pins have 25ns of rise/fall time on their board.

Could you show me whether the 25nS of rise/fall time is acceptable?

Thanks,

Miyamoto

0 Kudos
1 Solution
665 Views
igorpadykov
NXP Employee
NXP Employee

Hi AVNET JAPAN FAE

rise/fall times are not specified, because they are not important.

Important are setup and hold times, these and other important parameters

are provided in datasheet.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
666 Views
igorpadykov
NXP Employee
NXP Employee

Hi AVNET JAPAN FAE

rise/fall times are not specified, because they are not important.

Important are setup and hold times, these and other important parameters

are provided in datasheet.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
665 Views
Aemj
Contributor IV

Dear Igor,

Thanks for your prompt reply.

Can i understand 25nS of rise/fall time is OK?

My customer wants your comment on the rise/fall time.

BR,

Miyamoto

0 Kudos
665 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

yes this rise/fall time is OK.

~igor

0 Kudos