Question about i.MX6 PCIe endpoint?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about i.MX6 PCIe endpoint?

2,924件の閲覧回数
nickyang
Contributor I

Hi,

I would like to use i.MX6 PCIe as endpoint and Windows PC's PCIe as RC (Root Complex) and transfer raw 1080p60 YUV422 video from i.MX6 board's video input to PCIe, then to PC. My questions are:

1) Has anybody done such as a system (i.MX6 PCIe as endpoint and Windows PC's PCIe as RC)?

2) i.MX6 PCIe is fast enough to transfer 1080p60 YUV422 video data to PC?

3) When i.MX6 PCIe is used as endpoint, do I need to worry about Window's side PCIe driver? Or i.MX6 can be recognized by Windows automatically?

4) Can the above job be done with an i.MX6 solo? Or I have to use i.MX6 Quad?

Thanks in advance,

Nick

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,651件の閲覧回数
nickyang
Contributor I

Hi, Igor.

Thanks for the reply. I already checked that document. Since that test was done in 2013, I assume 300MB/s feature is supported in the current i.MX6 Linux distribution so I don't need to develop "my own special driver" to support 300MB/s transfer rate. Is it correct?

Do you know any of your customer used i.MX6 PCIe as endpoint to plug into Windows PC PCIe as RC? From my research, most of people use i.MX6 PCIe as RC.

Thanks,

Nick

0 件の賞賛
返信

2,651件の閲覧回数
hey_sally
Contributor I

Hi Nick,

Have you worked out the  i.MX6 PCIe with Windows PC successfully ?

We are now having a project , the same application as your.

Can you share some of your experience ?

Thanks

Sally

0 件の賞賛
返信

2,651件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nick

unfortunately I am not aware of efforts of using i.MX6 PCIe with Windows PC, sorry.

Best regards
igor

0 件の賞賛
返信

2,651件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nick

seems special driver should be developed and one can start with example on

https://community.freescale.com/docs/DOC-95014 

it shows throughput perfomance about 300MB/s which in general may be sufficient for

1080p60 YUV422. There are no restrictions for using i.MX6S, choice depends on other

tasks which may affect overall processor bus loading.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信