Question about i.MX53 DDR3 Script Aid

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about i.MX53 DDR3 Script Aid

2,809件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I want to confirm about i.MX53 DDR3 Script Aid.

I downloaded it from below thread.

https://community.freescale.com/docs/DOC-102457

In my understanding, if user set some information in "Register Configuration" tab, the register values are changed in "RealView.inc" tab.

But some register values are never changed (e,g ESDREF).

Does it proper operation ?

If you know something about it, please tell me.

ko-hey

ラベル(1)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

2,442件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, the i.MX53 DDR3 Script Aid is very simplified, and it does not

support fine tuning of DDR parameters.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,442件の閲覧回数
ko-hey
Senior Contributor II

Hi Yuri

So user have to change themselves ?

Ko-hey

0 件の賞賛
返信

2,442件の閲覧回数
Yuri
NXP Employee
NXP Employee

You can request more detailed xls via SR.

Regards,

Yuri.

0 件の賞賛
返信

2,442件の閲覧回数
ko-hey
Senior Contributor II

OK, I'll ask to SR.

ko-hey

0 件の賞賛
返信