Question, MC34704 VIN current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, MC34704 VIN current

1,282件の閲覧回数
Aemj
Contributor IV

Hello team,

I have a customer who is using MC34704 with i.MX25.

And 5V is supplied into VIN of MC34704, and REG2,3,4 are used on his board.

In that case, where can I find the description which can be helpful to estimate the current flowing into PVIN2,3,4(VIN)?

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 返信

1,224件の閲覧回数
art
NXP Employee
NXP Employee

The estimation is quite simple in that case. Let's consider it on "per regulator" basis.

1. First, calculate the power that the regulator 'x' provides to a load: Pout_x = Vout_x * Iout_x, where Pout_x is the output power of a regulator 'x', Vout_x and Iout_x - its output voltage and current, respectively.

2. Then, assuming the typical conversion efficiency of regulator as 80% (denoted in the data sheet), multiply the Pout_x by 1.25 (1/0.8) to calculate the power that the regulator 'x' consumes on its input: Pin_x = Pout_x *1.25 .

3. Now, knowing the input power and input voltage, we can calculate the input current: Iin_x = Pin_x / Vin_x .

Assuming the input voltage of 5V, the final calculation for a regulator 'x' is as follows:

Iin_x = (Vout_x * Iout_x * 1.25) / 5 = (Vout_x * Iout_x) / 4 .


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信