Question, APP for i.MX6SoloX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, APP for i.MX6SoloX

1,468件の閲覧回数
SLICE
Contributor IV

Dear team,

I would like to ask about APP(Adjusted Peak Performance) value of i.MX6SoloX.

We already know that NXP does not provide such numbers regarding to the performance of SOC.

But my customer needs to know how to calculate it due to their company policy.

They believes that the below formula is the one for i.MX6SoloX chip.

 

APP = 1 (one Cortex-A9) * 1 (GHz) * 1 (FPO for CA9) * 0.3 (W) * 10^-3 +

      1 (one Cortex-M4) * 0.277 (GHz) * 0.277 (FPO for CM4) * 0.3 (W) * 10^-3

The first line of the above formula is corresponding to Cortex-A9 and the second line is corresponding to Cortex-M4. 

Is it correct?

They have a little concern that 2.277 of FPO for CM4 is really correct or not.

Best Regards,

Miyamoto

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,293件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Miyamoto San,

As you well mention,  NXP does not provide APP  numbers,  regarding your question from the metric,   I understand that Processors without 64 bit (or better) floating point support have an FPO of zero.  This is the case of the M4 so I would put an FPO =0.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,293件の閲覧回数
SLICE
Contributor IV

Hello jamesbone‌

Thanks for your support.

Can I understand that the following formula can calculate APP of i.MX6SoloX?

APP = 1 (one Cortex-A9) * 1 (GHz) * 1 (FPO for CA9) * 0.3 (W) * 10^-3 

Best Regards,

Miyamoto

0 件の賞賛
返信