[Qt5 - iMX6] How to add the support of look and feel of Qt in eglfs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[Qt5 - iMX6] How to add the support of look and feel of Qt in eglfs

915 次查看
vincentbodin
Contributor II

Hi,

Sorry but maybe this question is probably not in the right place...

I've recently try the QT5Cinematic demo on my iMX6 board through eglfs and it works like a charm.

Now, I'm currently desiging a Qt application with Qwidget support. Unfortunately, when I add a button to the MainWindo.ui, this button doesn't look like it has to be (the look and feel is not very beautiful...). That's the same thing for the Mainwindow.

How to proceed to enable the Qt look and feel in my application ?

Thanks, Vincent

PS : I use the core-image-minimal of Yocto FSL communty BSP

标签 (2)
标记 (3)
0 项奖励
回复
1 回复

755 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vincent

as this is specific Qt question suggest to post it on special Qt forums

like I.MX-6 - Qt Wiki

Best regards

igor

0 项奖励
回复