QSPI boot from ROM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QSPI boot from ROM

1,241 Views
ani10c89
Contributor II

In iMX8M reference schematics, it is mentioned that QSPI boot is not supported by ROM. Does it mean that QSPI booting has some issues ? I didn't find any information on this in Errata or RM. Please confirm.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,110 Views
art
NXP Employee
NXP Employee

Yes, you are right, the QSPI boot is not supported in the current Boot ROM code revision. Most likely, will be implemented in further silicon releases.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply