QSPI boot from ROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QSPI boot from ROM

1,315件の閲覧回数
ani10c89
Contributor II

In iMX8M reference schematics, it is mentioned that QSPI boot is not supported by ROM. Does it mean that QSPI booting has some issues ? I didn't find any information on this in Errata or RM. Please confirm.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,184件の閲覧回数
art
NXP Employee
NXP Employee

Yes, you are right, the QSPI boot is not supported in the current Boot ROM code revision. Most likely, will be implemented in further silicon releases.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信