QDIDs Bluetooth BLE and A2DP - help and advice

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QDIDs Bluetooth BLE and A2DP - help and advice

1,768 Views
edwardtyrrell
Senior Contributor I

Hi,

Does anyone know the BLE and A2DP QDIDs that are associated with the imx7s using Blue5.47 (on Linux 4.1) and the iMX7d using Bluez 5.46 (on Linux 4.9.88)? Both Yocto FSL Builds.

We're totally in the dark knowing how to obtain these for certification. Any help or information would be greatly appreciated. We have the WiFi/BT module's QDID but that differs according to BT SIG from these higher level QDIDs.

 

Thanks,

 

0 Kudos
Reply
1 Reply

1,728 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @edwardtyrrell, 

The QDID is related to the WiFI/BT module, and you mentioned that you already have the QDID for these modules.
Also, the information related to QDID could be private information I would recommend creating a support ticket, here our internal team specializing in Bluetooth Technology will provide more information.

This is the link to create a support ticket: Support | NXP Semiconductors

Have a great day!

Best regards, Brian.

0 Kudos
Reply