Programming SPI via mfgtools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming SPI via mfgtools

1,617 Views
pt
Senior Contributor I

Hi

I have used mfgtools to program spi. But I am getting the following error.

 

Log:

Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE

 

Panel A UtpUpdate Event: VolumeArrival Msg: (null) DevState: Updater OpState: WAITING_FOR_DEVICE

 

1 - Panel A Finished <CMD/> type="find" body="Updater" file="" timeout="180" onError="" text="" SUCCESS code=0x0.

 

Panel A Start <CMD/> type="push" body="mknod class/mtd,mtd0,/dev/mtd0" file="" timeout="10" onError="" text="".

 

1 - Panel A Finished <CMD/> type="push" body="mknod class/mtd,mtd0,/dev/mtd0" file="" timeout="10" onError="" text="" FAIL code=0xffffffff.

 

Panel A: Operation is not completed.,failed to run command: type="push" body="mknod class/mtd,mtd0,/dev/mtd0" file="" timeout="10" onError="" text="" 

 

2 - Panel A Finished processing SPI-NOR (uboot.sb) <LIST/> : FAIL code=-1.


Board:MCIMX28EVK

Linux2.6.35 kernel version

SPI flash:N25Q128


Regards

Pt

Original Attachment has been moved to: spi-log.txt.zip

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

1,282 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I checked one version of mfgtool and it seems that it does not support SPI NOR.  I wonder if you checked the below discussion.

How to enable SPI NOR boot for i.MX28 (Spansion s25fl256s)

It contains the required steps to add the the SPI NOR support.

Best Regards,

Alejandro

0 Kudos
Reply