Problem with the network manager

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with the network manager

2,097 Views
rajspatel1297
Contributor I

Hi, 

I'm just wondering that why in the boot sequence, there are two services with NetworkManager named with LSB.

Starting Network Manager...

Starting LSB: network connection manager...
[ OK ] Started Login Service.
[ OK ] Started Network Manager.
[ OK ] Started LSB: network connection manager.
[ OK ] Reached target Network.

Moreover the output of the systemctl --type=service contains two network manager services

network-manager.service loaded active exited LSB: network connection manager 
NetworkManager-wait-online.service loaded active exited Network Manager Wait Online
NetworkManager.service loaded active running Network Manager

Can someone please explain it?

 

Labels (1)
0 Kudos
Reply
3 Replies

2,087 Views
jimmychan
NXP TechSupport
NXP TechSupport

Which board are you using?

Which version of BSP are you using?

 

0 Kudos
Reply

2,083 Views
rajspatel1297
Contributor I

I’m using compulab cl-som-imx7 board with Dunfell version.

 

https://github.com/compulab-yokneam/compulab-fslc-bsp/tree/dunfell

0 Kudos
Reply

2,078 Views
jimmychan
NXP TechSupport
NXP TechSupport

In our BSP, we don't have this network manager. As the BSP package is board specific, you may contact the support of Compulab for this network manager issues.

0 Kudos
Reply