Problem with nand flash programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with nand flash programming

2,877 Views
alessandrobenfe
Contributor I

Hi, i work with two SOM one with imx6solo and other one with imx6quad, both SOM have with same nand flash.

With a MicroSD card update the SOM; with imx6quad I always have success, but with imx6solo sometimes don't have success.

For update the rootfs I use a script with this instructions:
ubiformat -y /dev/mtd3
ubiattach /dev/ubi_ctrl -m 3
ubimkvol /dev/ubi0 -N rootfs -s445000000
mkdir /rootfs
mount -t ubifs ubi0:rootfs /rootfs
tar xvf /rootfs.tar.bz2 -C /rootfs
sync

When I boot from nand flash I have some errors of this type:

UBIFS error (ubi0:0 pid 277): ubifs_read_node: bad node type (255 but expected 1)
UBIFS error (ubi0:0 pid 277): ubifs_read_node: bad node at LEB 394:119808, LEB mapping status 0
Not a node, first 24 bytes:
00000000: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ........................

I don't understand what the problem could be due to and what settings to check.

Note: I use a yocto pyro distribution

 

Can you help me?

Thanks,

Alessandro

Labels (2)
0 Kudos
Reply
3 Replies

2,768 Views
kef2
Senior Contributor V

FF FF.. looks like erased flash page. It could be for example due to misconfigured U-Boot environment area in NAND flash, so that when U-Boot stores environment variables, NAND page(s) at bottom of your UBI partition gets erased.

0 Kudos
Reply

2,772 Views
alessandrobenfe
Contributor I

Hi,

from the tests carried out the error seems to occur due to the use of two different distributions of yocto to create the OS of the microSD and the one contained in the flash.

For the quad core version the same version of yocto was used for both the microSD and the flash.

I believe there is some incompatibility between the versions of the flash management drivers between the two kernel versions used in the yocto distributions.

At the moment, by using the same version of yocto to build the OS for everyone we solved the problem.

0 Kudos
Reply

2,844 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Check your SOM vendor because apparently t does not use the same nand on both MX6 processors.

Regards

0 Kudos
Reply