Problem installing extra-cmake-modules into sdk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem installing extra-cmake-modules into sdk

1,998 Views
BJ125
Contributor I

I am trying to install "extra-cmake-modules" package into the sdk.

First, I added this into "local.conf":

      IMAGE_INSTALL += "extra-cmake-module
and the "populate_sdk" will build the sdk, but it went into target part of the sdk. If I try to use a cmake module, it says that it can't find it. Of course, since it went into the target part of the sdk.

Then I used this:

     TOOLCHAIN_HOST_TASK += "extra-cmake-modules"

and the "populate_sdk" fails with the error:

Sstate summary: Wanted 2 Local 0 Mirrors 0 Missed 2 Current 3329 (0% match, 99% complete)################################################################################################################                    | ETA:  0:00:00
Initialising tasks: 100% |###################################################################################################################################################################################################| Time: 0:00:04
NOTE: Executing Tasks
ERROR: imx-image-multimedia-1.0-r0 do_populate_sdk: Unable to install packages. Command '/home/dejovivl/external_disk/imx95_image/vhip_way_image/poky/build/tmp/work/ifm_imx95_19x19_verdin-poky-linux/imx-image-multimedia/1.0/recipe-sysro
ot-native/usr/bin/apt-get  install --allow-downgrades --allow-remove-essential --allow-change-held-packages --allow-unauthenticated --no-remove  extra-cmake-modules' returned 100:
Reading package lists...
Building dependency tree...
Reading state information...                                                                                                                                                                                                                 
E: Unable to locate package extra-cmake-modules                                                                                                                                                                                              
                                                                                                                                                                                                                                            
ERROR: Logfile of failure stored in: /home/dejovivl/external_disk/imx95_image/vhip_way_image/poky/build/tmp/work/ifm_imx95_19x19_verdin-poky-linux/imx-image-multimedia/1.0/temp/log.do_populate_sdk.342802
ERROR: Task (/home/dejovivl/imx95-image/meta-imx/meta-imx-sdk/recipes-fsl/images/imx-image-multimedia.bb:do_populate_sdk) failed with exit code '1'
NOTE: Tasks Summary: Attempted 7593 tasks of which 7592 didn't need to be rerun and 1 failed.


That means you got a bug in this bb file. So, what do I need to do to install this package into the host part of the sdk?

 

0 Kudos
Reply
2 Replies

1,956 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Please note that the i.MX95 is still in pre-production stage so we cannot offer support to it, please contact your local Sales/FAE for further assistance.

Best regards/Saludos,
Aldo.

0 Kudos
Reply

1,942 Views
BJ125
Contributor I

That is not very helpful. Regardless of whether it is preproduction or not, I put a link to the recipe that comes from NXP, and someone there could take a look.

What is a way to report a bug for that recipe? If I find a way to fix it, how to send them a patch?

0 Kudos
Reply