Power management Power consumption : ARM Core off

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power management Power consumption : ARM Core off

ソリューションへジャンプ
5,181件の閲覧回数
cader
Contributor II

Dear Freescale Support Team,

We are working on the Power management Module on i.MX6Q Based SabreSDP Platform with B5 Revision and the Processor Revision is 1.2(i.e AC)

We would like to know about the ARM Power off sequence in i.MX6q and any one has the procedure to Enter in to the ARM Power off state please share.

And i would like to know any other module dependency with ARM Power off . What is the power consumption will reduce if ARM Power off performed in the SabreSDP Platform.

Any other documentation for suspend and resume what is the exact procedure. How to make sure ARM is in Power OFF mode.

Best Regards,

Cader.

ラベル(2)
0 件の賞賛
返信
1 解決策
2,668件の閲覧回数
Yuri
NXP Employee
NXP Employee

As for power consumption please use the next app notes :

http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf

http://cache.freescale.com/files/32bit/doc/app_note/AN4576.pdf

The mentioned app notes relate to Linux BSP :


https://www.freescale.com/webapp/Download?colCode=L3.0.35_1.1.0_SOURCE&appType=license&location=null


https://www.freescale.com/webapp/Download?colCode=L3.0.35_3.0.0_ER_SOURCE&appType=license&location=n...


Please use Linux documentation for information about source files, responsible

for power saving modes.


https://www.freescale.com/webapp/Download?colCode=L3.0.35_1.1.0_LINUXDOCS_BUNDLE&location=null


In particular, please look at  Chapter 16 "Low-level Power Management (PM) Driver"

of "Linux_6DQ_RM_L3.0.35_1.1.0.pdf".


Also the SDK contains examples. 

Please look at Chapter 24 (Configuring the Power Modes) of "iMX6_Firmware_Guide.pdf".


https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,669件の閲覧回数
Yuri
NXP Employee
NXP Employee

As for power consumption please use the next app notes :

http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf

http://cache.freescale.com/files/32bit/doc/app_note/AN4576.pdf

The mentioned app notes relate to Linux BSP :


https://www.freescale.com/webapp/Download?colCode=L3.0.35_1.1.0_SOURCE&appType=license&location=null


https://www.freescale.com/webapp/Download?colCode=L3.0.35_3.0.0_ER_SOURCE&appType=license&location=n...


Please use Linux documentation for information about source files, responsible

for power saving modes.


https://www.freescale.com/webapp/Download?colCode=L3.0.35_1.1.0_LINUXDOCS_BUNDLE&location=null


In particular, please look at  Chapter 16 "Low-level Power Management (PM) Driver"

of "Linux_6DQ_RM_L3.0.35_1.1.0.pdf".


Also the SDK contains examples. 

Please look at Chapter 24 (Configuring the Power Modes) of "iMX6_Firmware_Guide.pdf".


https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null

0 件の賞賛
返信
2,668件の閲覧回数
Oceanblue
Contributor III

Hi Yuri,

      Could you please explain a little detail about Power off sequence? we have met the same problem, and expect to port it on ourselves power management circuit. thanks

JK W

0 件の賞賛
返信
2,668件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please look at section 5 (Use case configuration and usage guidelines) of app note AN4576 (i.MX 6DualLite Power Consumption Measurement), in particular, for Deep-Sleep mode :

echo mem > /sys/power/state

0 件の賞賛
返信