What exactly are them recent Linux kernel patches available post the rel_imx_5.4.70_2.3.2 tag?
https://source.codeaurora.org/external/imx/linux-imx/log/?h=imx_5.4.70_2.3.0
Are they related to the recently released Linux 5.4.70_2.3.3 Patch?
Or what exactly are those about?
Does NXP plan to do another official release that includes them (and tag them)?
Hello marcelziswiler,
Those are patches exclusively for the nxp hardware side and they were include in the L5.10 release. There is no plan to be included in 5.4.70.
Release