Post rel_imx_5.4.70_2.3.2 Linux Kernel Patches on imx_5.4.70_2.3.0 Branch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Post rel_imx_5.4.70_2.3.2 Linux Kernel Patches on imx_5.4.70_2.3.0 Branch

1,061件の閲覧回数
marcelziswiler
Senior Contributor I

What exactly are them recent Linux kernel patches available post the rel_imx_5.4.70_2.3.2 tag?

https://source.codeaurora.org/external/imx/linux-imx/log/?h=imx_5.4.70_2.3.0

Are they related to the recently released Linux 5.4.70_2.3.3 Patch?

Or what exactly are those about?

Does NXP plan to do another official release that includes them (and tag them)?

1 返信

1,054件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello marcelziswiler,

Those are patches exclusively for the nxp hardware side and they were include in the L5.10 release. There is no plan to be included in 5.4.70.

 

Release

 

 

 

0 件の賞賛
返信