Possible issue with iMX6 Platform SDK stack alignment at startup.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Possible issue with iMX6 Platform SDK stack alignment at startup.

Jump to solution
4,885 Views
EdSutter
Senior Contributor II

I've been wrestling with stability issues as I am trying to reuse portions of the iMX6 Platform SDK in my boot loader.  What I've found is that the memory map setup and the way stack is initialized, its possible that the stack pointer will not be double-word aligned.  Apparently it is important to start off with this double-word alignment, because I've found that when I build my boot loader and the "top_of_stack" location is NOT double-word aligned (divisible by 8), then my system doesn't boot; however, if I adjust the memory map to force that to a double-word aligned address it does boot.

While I don't fully understand the need for this double-word alignment, there is some information here...

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.faqs/ka4127.html

Anyway, the easy fix for this is to simply force this alignment in the linker file...

    .stacks (NOLOAD) :

    {

       . = ALIGN (8);          <<<<<< Add this line

        __stacks_start = .;

        . += 48K;

        __stacks_end = .;

        top_of_stacks = .;

    } > DDR

This apparently is not a problem for folks using the SDK (perhaps something else in the build is forcing this alignment that I'm not aware of), so I'd like to get feedback on this post to see if folks agree or disagree with this suggested change.

Tags (1)
0 Kudos
Reply
1 Solution
4,473 Views
EdSutter
Senior Contributor II

Right!

The quick fix is to do the ALIGN(8) that I show at the top.

The better fix is to apply the BIC instruction to all assignments of SP in that startup.S code...

   @ set stacks for all other modes

   msr     CPSR_c, #MODE_FIQ | I_BIT | F_BIT

   bic     r0, r0, #15

   mov     sp, r0

   sub     r0, r0, r1

   msr     CPSR_c, #MODE_IRQ | I_BIT | F_BIT

   bic     r0, r0, #15

   mov     sp, r0

   sub     r0, r0, r1

   msr     CPSR_c, #MODE_ABT | I_BIT | F_BIT

   bic     r0, r0, #15

   mov     sp, r0

   sub     r0, r0, r1

   msr     CPSR_c, #MODE_UND | I_BIT | F_BIT

   bic     r0, r0, #15

   mov     sp, r0

   sub     r0, r0, r1

   msr     CPSR_c, #MODE_SYS | I_BIT | F_BIT

   bic     r0, r0, #15

   mov     sp, r0

   sub     r0, r0, r1

   @ Set SVC mode stack with interrupts disabled

   msr     CPSR_c, #MODE_SVC | I_BIT | F_BIT

   bic     r0, r0, #15

   mov     sp, r0

   sub     r0, r0, r1

View solution in original post

0 Kudos
Reply
6 Replies
4,473 Views
maheshmahadeva1
NXP Employee
NXP Employee

Found the below code in sdk/core/src/startup.S which should take care of this:

/*
* fill the stacks with a pattern
* the stack must be 8 byte aligned
*/
ldr r1,=__stacks_start  @ stack region start address
ldr r2,=top_of_stacks   @ stack region end address
bic r2,r2,#0x7          @ round length down to nearest 8 byte alignment
ldr r3,=.Ldeadfeed      @ get fill pattern address
ldr r3,[r3]             @ read fill pattern into r3
mov r4,r3               @ copy fill pattern to r4
1:  cmp r1,r2               @ the fill loop
stmltia r1!,{r3-r4}
blt 1b

Best regards,

-Mahesh


0 Kudos
Reply
4,473 Views
EdSutter
Senior Contributor II

This does initialize the stack (which is good), but the important thing here is that the stack pointer itself be initialized with a value that is aligned.  So I think my original post (showing the ALIGN(8) in the loader file) actually solved the problem for me. Actually, in my boot monitor code, I use the BIC instruction to adjust what ultimately is used as the stack pointer... 

    ldr     r0, = (MonStack + MONSTACKSIZE - 4)

    bic r0, r0, #15

    mov     sp, r0

Doing it this way (in code, rather than depending on an aligned tag) eliminates the need to care where the stack memory is.  If you disagree, please let me know.  I've had this fix in place for weeks now and it has been working just fine.

0 Kudos
Reply
4,473 Views
maheshmahadeva1
NXP Employee
NXP Employee

Looks like the SDK misses aligning the address written to sp.

Best regards,

-Mahesh

0 Kudos
Reply
4,474 Views
EdSutter
Senior Contributor II

Right!

The quick fix is to do the ALIGN(8) that I show at the top.

The better fix is to apply the BIC instruction to all assignments of SP in that startup.S code...

   @ set stacks for all other modes

   msr     CPSR_c, #MODE_FIQ | I_BIT | F_BIT

   bic     r0, r0, #15

   mov     sp, r0

   sub     r0, r0, r1

   msr     CPSR_c, #MODE_IRQ | I_BIT | F_BIT

   bic     r0, r0, #15

   mov     sp, r0

   sub     r0, r0, r1

   msr     CPSR_c, #MODE_ABT | I_BIT | F_BIT

   bic     r0, r0, #15

   mov     sp, r0

   sub     r0, r0, r1

   msr     CPSR_c, #MODE_UND | I_BIT | F_BIT

   bic     r0, r0, #15

   mov     sp, r0

   sub     r0, r0, r1

   msr     CPSR_c, #MODE_SYS | I_BIT | F_BIT

   bic     r0, r0, #15

   mov     sp, r0

   sub     r0, r0, r1

   @ Set SVC mode stack with interrupts disabled

   msr     CPSR_c, #MODE_SVC | I_BIT | F_BIT

   bic     r0, r0, #15

   mov     sp, r0

   sub     r0, r0, r1

0 Kudos
Reply
4,473 Views
PaulDeMetrotion
Senior Contributor I

What is the file name to be edited?

0 Kudos
Reply
4,473 Views
EdSutter
Senior Contributor II

Under the sdk directory:

apps/common/basic_sdk_app.ld.S

0 Kudos
Reply