Poor Performance - i.MX53 Qt 4.7.4, hellogl_es2 example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Poor Performance - i.MX53 Qt 4.7.4, hellogl_es2 example

3,031 次查看
DD1z
Contributor II

Hi,

I am getting really poor performance on the i.MX 53 with Qt4.7.4 and the hellogl_es2 example.

The fps is showing about 13 fps. I installed Qt with the X-server.

The screen resolution is 1024x786.

Any ideask, why the performance is so poor?

标记 (2)
0 项奖励
回复
5 回复数

2,649 次查看
santiagoperez
Contributor I

HI DD1z,

could you fix the problem?. I'm having the same issue, even worst, just 6fps.

Regards

0 项奖励
回复

2,649 次查看
KrishnaPavan
Fresh Out Contributor

on i.MX51 amd-gpu-bin-mx51

0 项奖励
回复

2,649 次查看
santiagoperez
Contributor I

Could you run Qt over the frame buffer with GPU enabled?. I had no success and in several posts it is said you need to enable a specific plugin.

Thanks in advance,

0 项奖励
回复

2,649 次查看
DD1z
Contributor II

Which screen driver are you using?

0 项奖励
回复

2,649 次查看
KrishnaPavan
Fresh Out Contributor

I use without X11 libs and it's working fine.

0 项奖励
回复